SIP32455DB-T2-GE1 by Vishay Intertechnologies

Overview of SIP32455DB-T2-GE1 by Vishay Intertechnologies

The SIP32455DB-T2-GE1 is a single-pole single-throw (SPST) switched voltage regulator integrated circuit (IC) designed for various power management applications. The component falls under the subcategory of Power Management Circuits within the broader category of Power Circuits, indicating its role in regulating voltages efficiently throughout electronic systems. This part is actively manufactured by Vishay Intertechnologies, a well-known name in the electronics industry.

Regarding its operational attributes, it is important to note that the SIP32455DB-T2-GE1 adheres to various compliance codes, including the EAR99 ECCN code, which indicates that it is subject to Export Administration Regulations but does not require a specific export license. Additionally, it carries an HTS Code of 8542.39.00.01, which relates to the classification of electronic components. As of the current writing, the factory lead time for acquiring this part is approximately 14 weeks, requiring careful planning for procurement, especially in projects with tight schedules. Its lifecycle is categorized as ‘Active,’ suggesting ongoing production and availability for future projects.

Industry Applications for SIP32455DB-T2-GE1

The SIP32455DB-T2-GE1 might find utility in various industry sectors due to its functionality as a voltage regulator. Here are some potential applications where the part might be used:

  • Energy and Power Systems: In energy management systems, the SIP32455DB-T2-GE1 might be utilized to regulate voltages from renewable energy sources, such as solar panels, ensuring that the output voltage remains stable for further processing or storage. This component could potentially enhance energy quality and reliability in power systems that require precise voltage control.
  • Transportation and Logistics: The part could possibly be integrated into logistics and transportation systems for vehicle power management. In electric and hybrid vehicles, the SIP32455DB-T2-GE1 might be used in battery management systems to maintain stable voltages, prolonging battery life and optimizing performance.
  • Renewable Energy: Within renewable energy installations, such as wind turbines or solar photovoltaic systems, this component might help in the voltage regulation of outputs, thereby contributing to the overall efficiency of energy conversion systems. By ensuring that voltage outputs remain within specific parameters, the part can protect sensitive equipment from voltage spikes.
  • Automotive: If automotive industry standards like AEC-Q100 or AEC-Q101 are adhered to, the SIP32455DB-T2-GE1 might potentially be considered for use in automotive power management systems, particularly in applications requiring reliable voltage regulation for electronic control units or infotainment systems.
  • Consumer Electronics: While not listed in the potential applications, it is plausible that this voltage regulator could be implemented in consumer electronics that require stable power for performance, such as laptops and smartphones, where battery fuel efficiency is crucial.

It is important to note that these potential applications are only conceptual and illustrative. Engineering and design teams must conduct thorough analyses and verifications to ensure adherence to industry standards and specific application requirements before implementation.

About Vishay Intertechnologies

Vishay Intertechnologies is a prominent manufacturer specializing in various electronic components, including those within the Power Management Circuits segment. The company has a dedicated focus on producing high-quality power management solutions, delivering components designed to meet a wide range of applications across multiple industries.

The SIP32455DB-T2-GE1 represents a portion of Vishay’s extensive portfolio, which includes similar parts that might assist in managing power efficiently. Vishay’s commitment to quality and performance is encapsulated in its rigorous testing and adherence to industry compliance standards, making their products suitable for various applications requiring reliable voltage management and regulation.

Where to Find SIP32455DB-T2-GE1 by Vishay Intertechnologies

To procure the SIP32455DB-T2-GE1, interested buyers should research purchasing options on findchips.com. The platform can help locate this voltage regulator and provides insights into stock levels, pricing, and availability.

Historically, the part has been available through several distributors, including:

  • EBV Elektronik
  • TTI
  • Mouser Electronics
  • Future Electronics
  • Avnet Americas

It is advisable to consult findchips.com for current stock levels and pricing, ensuring that stakeholders can make informed procurement decisions.

Compare pricing for SIP32455DB-T2-GE1 and other Power Management Circuits / Power Circuits at findchips.com