SS02-0B00-00 by Broadcom Limited

Overview of SS02-0B00-00 by Broadcom Limited

The SS02-0B00-00 is a PCI Bus Controller manufactured by Broadcom Limited, designed to facilitate communication between the central processing unit (CPU) of a computer and its connected devices, through the Peripheral Component Interconnect (PCI) bus. With its technology based on Complementary Metal-Oxide-Semiconductor (CMOS), this electronic component offers a reliable solution for managing the data transfer between the PCI bus and other bus standards. Noteworthy, as of the current writing, this part has a factory lead time of 50 weeks, indicating a consideration for planning in procurement strategies.

Industry Applications for SS02-0B00-00

The SS02-0B00-00 may find applications across a wide range of industries due to its fundamental role in enabling communication over the PCI bus. Some potential applications include:

  • Computing and Data Storage: It could serve as an essential component in desktop computers, servers, and data storage systems, facilitating rapid data transfer and improving overall system performance.
  • Internet of Things (IoT): Given the growing need for connectivity in IoT devices, this PCI bus controller may be suitable for use in IoT gateways and hubs, allowing for efficient data handling between various sensors and the central processing unit.
  • Aerospace and Defense: The reliability and performance of this component make it potentially suitable for applications in aerospace and defense, where robust and efficient data communication systems are crucial.
  • Automotive: In the automotive industry, the SS02-0B00-00 could be used in vehicle diagnostics or infotainment systems, needing high-speed data transmission between various system components.

These applications highlight the versatility and importance of the SS02-0B00-00 in various high-tech sectors, underscoring the component’s contribution to enabling efficient and reliable data communication.

About Broadcom Limited.

Broadcom Limited, formerly known as Avago Technologies, is a global leader in the development and manufacturing of a wide range of semiconductor and infrastructure software solutions. In the realm of Microcontrollers and Processors, and specifically within the subcategory of Bus Controllers, Broadcom stands out for its high-quality and innovative products. The SS02-0B00-00, alongside similar parts, showcases Broadcom Limited’s commitment to delivering advanced technology solutions that meet the ever-evolving needs of the tech industry. Their products are integral in powering applications across diverse market segments, including telecommunications, data center, enterprise software, and more, reflecting the company’s footprint in pushing the boundaries of connectivity and infrastructure management.

Where to Find SS02-0B00-00 by Broadcom Limited

To procure the SS02-0B00-00, one recommended strategy is to conduct a search on findchips.com. This platform provides a comprehensive database of distributors along with current stock levels and pricing, making it an invaluable resource for technical engineering and procurement professionals. To explore alternatives or similar Bus Controllers manufactured by Broadcom Limited or other brands, visiting the Bus Controllers section on findchips.com can offer broader insights.

Distributors such as DigiKey, Avnet Americas, Mouser Electronics, Velocity Electronics, and EBV Elektronik have historically stocked the SS02-0B00-00. However, availability can fluctuate, and for the most current information on stock levels and competitive pricing, checking findchips.com directly is always the best approach.

Compare pricing for SS02-0B00-00 and other Bus Controllers / Microcontrollers and Processors at findchips.com