A Findchips sourcing guide.
Overview
Evaluating STM32 alternatives was once a practice adopted only during times of shortage. However, seeking second sources to STMicroelectronics’ ubiquitous 32-bit ARM Cortex-M based microcontroller family has now become a standard design practice, regardless of current availability conditions. Teams building anything with a service life longer than a couple of years are now expected to name a backup part during the schematic review phase.
Supplyframe’s demand picture reflects that shift. Our Design Insights data shows steady and broad development activity across the STM32F4 line, rather than a spike concentrated on one part number. This pattern is the signature of ongoing design-in activity rather than panic buying.
Search behavior matches this scenario. The STM32 family draws roughly 156,000 global searches per month, and a meaningful share of that traffic is comparison intent: Engineers are not asking what an STM32 does, but which one to use and what alternatives to fall back on.
This guide covers that decision process.
Next step: See how a candidate part is actually stocked before you commit to it. Compare STM32 microcontroller availability across distributors on Findchips
Start Inside the Family
Most second-sourcing problems are really selection challenges that were solved too narrowly in the past.
The STM32 line splits by series letter, and each letter provides a different answer to a different constraint. The F0 and G0 series are the value tier for simple control tasks. The F1 series is legacy, but is still specified frequently because so much reference code uses it.
The F4 series is the mainstream performance tier, which is why the STM32F407 keeps appearing in new designs. The G4 series targets mixed signal and motor control tasks with better analog integration. The H7 series represents the high-performance tier. The L4 and U5 series exist for designs with battery budgets, while the WB and WL series fold in wireless capabilities.
Within a series, the part number itself encodes the flexibility you have. The MPN includes a letter for pin count, a letter for flash memory size, a letter for package, and a digit for temperature grade. That structure matters because it means a shortage of one suffix often has an answer two characters away, on the same footprint, running the same firmware. As a result, moving from a 512 KB flash variant to a 1 MB variant in the same package is a sourcing decision, not a redesign.
Buyers should make sure they understand which MPN is most most suitable before selecting a vendor. Our STM32F407 specs, variants, and sourcing guide describes what the suffixes mean for the highest volume part in the F4 series.
Where Alternate Vendors Actually Fit
GigaDevice is the closest thing to a like-for-like alternative. The company’s GD32F407 is positioned as near pin to pin with the STM32F407 and is largely software compatible, with more than a decade of volume production behind the broader GD32 line. Expect register-level differences in clock configuration and flash timing rather than a clean recompile.
Artery is the performance play, and this is where cross-reference lists get it wrong most often. Many of them name the AT32F403A as a STM32F407 substitute. While the AT32F403A is a strong part, featuring a Cortex-M4F running up to 240 MHz on a footprint aligned with the smaller STM32 packages, it lacks an Ethernet MAC.
If your F407 design uses the Ethernet controller, as a large share of industrial F407 designs do, the part you actually want is the AT32F407, which adds a 10/100 Mbps Ethernet MAC with IEEE 1588 support and MII or RMII selection on top of the same core and clock. That single peripheral difference is the most common way an otherwise sound second-source plan fails.
WCH (Nanjing Qinheng Microelectronics) strays further from the STM32 on the compatibility front. The company’s CH32V307 pairs a RISC-V core with an integrated Ethernet PHY at a price point that makes it interesting for cost-driven designs. However, the CH32V307 represents a toolchain change, not a footprint swap. Treat it as a redesign candidate, not a drop-in replacement.
Worth Considering: Confirm whether an alternate is genuinely orderable through authorized channels before you design it in. Search GD32F407 distributor stock on Findchips
Comparing the Candidates
| Candidate | Core and max clock | Key difference versus STM32F407 | Best fit |
|---|---|---|---|
| STM32F407 | Cortex-M4 at 168 MHz | Baseline: a high-performance 32-bit RISC microcontroller. | Mainstream performance designs already validated on ST tooling |
| STM32F429 | Cortex-M4 at 180 MHz | Adds LCD-TFT controller and Chrom-ART | Same firmware base, needs a display path |
| GD32F407 | Cortex-M4 | Near pin to pin, software compatible with clock and flash timing differences | Closest hardware level second source |
| AT32F407 | Cortex-M4F at 240 MHz | Retains Ethernet MAC, higher clock, zero wait flash regions | Ethernet designs needing performance headroom |
| AT32F403A | Cortex-M4F at 240 MHz | No Ethernet MAC, smaller package range | Non-networked designs where clock speed matters |
| CH32V307 | RISC-V at 144 MHz | Different architecture and toolchain, integrated Ethernet PHY | Cost-driven redesigns, not footprint swaps |
Specifications should be confirmed against current datasheets before design lock, since vendors revise package and peripheral offerings across silicon revisions.
Next step: Put your shortlist through one availability check instead of six. Look up any of these part numbers on Findchips
Frequently Asked Questions
Is the GD32F407 a drop-in replacement for the STM32F407?
Close, but not automatic. The GD32F407 is positioned as near pin to pin and largely software compatible with the STM32F407, which usually means the PCB carries over unchanged. Firmware typically needs attention around clock tree configuration and flash wait states, and any peripheral driver written against ST register behavior should be retested rather than assumed.
Which Artery Part Matches an STM32F407 With Ethernet?
The AT32F407 matches, but the AT32F403A does not. Both are Cortex-M4F parts running to 240 MHz, but the Ethernet MAC is present only on the AT32F407. Cross-reference lists frequently name the AT32F403A as the F407 alternate, which works for designs that never used the Ethernet controller and fails immediately for designs that did.
Can I Second Source an STM32 Without Changing My PCB?
Often, yes, and the easiest path is inside the ST catalog. Different flash and RAM suffixes within the same series and package are usually footprint identical, so a supply problem on one variant can be answered by a variant two characters away. Alternate vendor parts vary: some hold the footprint, while others shift package options enough to require a layout revision.
How Do I Qualify an Alternate MCU Vendor for a Long Life Product?
Look at three factors beyond the datasheet. How long the substitute family has been in volume production, whether the vendor publishes a longevity or EOL commitment you can plan against, and whether your product needs automotive or functional safety qualification the alternate has not yet reached. A part that matches electrically can still fail a seven-year service life requirement on policy grounds alone.
Next step: Start the qualification with real distributor coverage rather than a datasheet alone. Compare authorized and independent stock on Findchips
The Bottom Line
Second sourcing an STM32 is a two-step decision, and most teams skip the first one. Before you evaluate another vendor, check the suffix axis inside the series you already chose, because a different flash or pin count variant on the same footprint is the cheapest hedge available and requires no requalification.
When the family itself is the exposure, the alternates are real but not interchangeable. The failure point is almost never the core. It is usually a peripheral that quietly did not come along.
Next step: Turn your second source shortlist into a sourcing decision today. Check live availability for your STM32 alternates on Findchips