Overview of STM32F042F6P6TR by STMicroelectronics
The STM32F042F6P6TR by STMicroelectronics features an Arm Cortex-M0 core, operating at a maximum frequency of 48 MHz. Included in its feature set are 32 KB of Flash memory, multiple communication interfaces such as USB and CAN, and Consumer Electronics Control (CEC) functions. This device is encapsulated in a TSSOP-20 package and is designed for a variety of applications that demand low-power performance combined with real-time functionalities. The chip supports a data bus width of 32 bits, ensuring efficient handling of operations.
This microcontroller is part of the STM32 family, specifically the STM32F0 series, known for their robustness and reduced system cost by integrating more features in smaller packages. The use of a high-performance Cortex-M0 processor allows this MCU to manage single-cycle multiplications and hardware division, an enhancement that makes it suitable for a wide range of applications. The STM32F042F6P6TR further supports a rich set of peripherals, including an internal 3-channel ADC, DMA channels, and multiple timers, facilitating complex peripheral management and enhanced task scheduling.
Industry Applications for STM32F042F6P6TR
Potential applications for the STM32F042F6P6TR span a diverse set of industries where integration, power efficiency, and cost-effectiveness are crucial. Notably, its involves sectors that require highly reliable, responsive, and capable processing solutions. Below are some potential industry applications for this microcontroller:
- Consumer Electronics: This microcontroller could be utilized in consumer gadgets such as wearables or home automation systems. Its low power consumption and USB capabilities make it an excellent choice for portable applications and devices requiring complex user interfaces.
- Industrial Automation: Its robust set of communication interfaces, including CAN for fieldbus networks, makes the STM32F042F6P6TR possibly suitable for industrial control systems, aiding in real-time process control and automation tasks that require reliable data transmission.
- Healthcare: In medical devices that need accurate sensor readings and secure communication, this microcontroller, with its built-in ADCs, might be effectively used. It can manage multiple sensor data integrations, vital in compact medical wearables or portable diagnostics equipment.
These potential industry applications are purely illustrative and require engineering and design teams to evaluate and confirm compliance with specific industry standards and application prerequisites.
About STMicroelectronics
STMicroelectronics is a global leader in semiconductor solutions, particularly noted for its strong portfolio in Microcontrollers and processors. The company serves a multitude of industries ranging from automotive to industrial, and its microcontroller lines, including the STM32 family of which the STM32F042F6P6TR is a part, are widely recognized for their scalability, performance, and power efficiency. STMicroelectronics continues to innovate in the field of embedded systems, with the STM32F042F6P6TR embodying the company’s commitment to providing advanced features and functionality that meet the growing demands of modern smart embedded applications.
Where to Find STM32F042F6P6TR by STMicroelectronics
To secure this specific microcontroller or evaluate other alternatives, leveraging a reliable source for component procurement is indispensable. Interested buyers can research and purchase the STM32F042F6P6TR on the platform findchips.com. This site helpfully aggregates current availability and pricing from multiple distributors and offers comparison charts for alternative products in the microcontroller category. Historically, distributors such as Mouser Electronics, DigiKey, and Avnet Americas, among others, have stocked this part. However, for real-time stock levels and the most competitive pricing, checking on findchips.com is recommended.
Other microcontrollers by STMicroelectronics or alternate manufacturers can also be explored through the comprehensive listings under Microcontrollers on findchips.com.