STM32F405RGT6TR by STMicroelectronics

Overview of STM32F405RGT6TR by STMicroelectronics

The STM32F405RGT6TR is a high-performance microcontroller unit (MCU) manufactured by STMicroelectronics, featuring the ARM Cortex-M4 core with a digital signal processor (DSP) and floating-point unit (FPU). This MCU is designed with a focus on performance, operating at a CPU frequency of up to 168 MHz. It uniquely integrates 1 Mbyte of Flash memory for storing applications and data, a significant capacity that supports complex operations and software frameworks. The inclusion of an ART Accelerator enhances its execution speed, reducing response time in critical applications.

This microcontroller is part of the broader category of Microcontrollers, specifically known for its low-power consumption backed by a range of power-saving modes. Its encapsulation in a 64-pin low-profile quad flat package (LQFP-64) ensures compactness and ease of integration into various designs, making it suitable for a wide range of electronic applications. It supports advanced connectivity, featuring multiple DMA channels, serial I/Os, and a wealth of peripherals that facilitate complex and flexible designs.

Beyond its core functionalities, this MCU is compliant with several regulatory standards such as RoHS, REACH, and ECCN, highlighting its broader acceptability in global markets. As of this writing, the factory lead time for STM32F405RGT6TR is approximately 16 weeks and 3 days, indicating its demand and production cycle for planning purposes.

Industry Applications for STM32F405RGT6TR

  • Internet of Things (IoT): With its advanced connectivity and low-power modes, STM32F405RGT6TR could serve as the brain of IoT devices, including smart sensors and actuators in smart home systems or industrial IoT solutions.
  • Consumer Electronics: In the realm of consumer electronics, this MCU might power devices that require high computational power and real-time processing, such as wearable technology or smart appliances.
  • Industrial Automation: The high performance and extensive I/O capabilities of STM32F405RGT6TR make it ideal for controlling complex industrial machinery or automation systems, where reliability and precision are crucial.
  • Robotics and Drones: Its capability to process complex algorithms quickly due to the DSP and FPU could make it suitable for the control systems of robots or drones, where rapid data processing and decision-making are essential.

These indicative applications highlight the versatility of STM32F405RGT6TR but require thorough analysis and verification by engineering and design teams to ensure suitability for specific projects.

About STMicroelectronics

STMicroelectronics is a global semiconductor leader that designs and manufactures a wide range of electronic components, including highly sophisticated Microcontrollers and Processors. The portfolio of STMicroelectronics is extensive, covering everything from simple control applications to complex digital ecosystems.

Within the realm of microcontrollers, STMicroelectronics is recognized for its STM32 family, which includes the STM32F405RGT6TR among other variants. These MCUs are characterized by their efficiency, robustness, and integration of advanced features such as DSPs, FPUs, and extensive memory options. STMicroelectronics’ products are instrumental in powering applications across automotive, industrial, IoT, and consumer electronics sectors, underscoring the company’s commitment to enabling smarter living and contributing to a sustainable future.

Where to Find STM32F405RGT6TR by STMicroelectronics

To source the STM32F405RGT6TR or explore alternative Microcontrollers that might suit specific application needs, Findchips.com is an invaluable resource. The website provides up-to-date availability, pricing, and datasheets from multiple distributors globally. Historically, this component has been available from distributors such as Win Source Electronics, Ameya Holding Limited, Bristol Electronics, and Avnet Americas. However, it’s crucial to visit Findchips for current stock levels and pricing to make an informed purchasing decision.

Compare pricing for STM32F405RGT6TR and other Microcontrollers / Microcontrollers and Processors at findchips.com