Overview of STM32F469IIT6 by STMicroelectronics
The STM32F469IIT6 is a high-performance microcontroller that employs an ARM Cortex-M4 core with digital signal processing (DSP) and a floating-point unit (FPU), enhancing its capability for handling complex algorithms and calculations. This component boasts 2 MBytes of Flash memory and a robust 180 MHz clock frequency. It is further enhanced by an ART Acceleratorâ„¢, Chrom-ART Acceleratorâ„¢ for advanced graphics, and comes with flexible memory controllers including FMC with SDRAM and Dual QSPI, which can greatly enhance its storage capabilities. For display and connectivity, it features interfaces like TFT and MIPI-DSI.
Manufactured by STMicroelectronics, one of the leaders in semiconductor solutions, this microcontroller is designed to accommodate demanding embedded applications due to its impressive array of features and performance specifications. As of the latest data from findchips.com, this part is classified as ‘Active’, and factory lead time is listed as 15 weeks.
Industry Applications for STM32F469IIT6
Considering its advanced features, the STM32F469IIT6 could seamlessly integrate into various high-demand sectors:
- Industrial Automation: This microcontroller could be employed in complex machinery controls, robotic systems, and process automation providing real-time performance and connectivity, supported by its high number of I/O lines and fast clock speed.
- Consumer Electronics: Its powerful graphics accelerators (ART and Chrom-ART) make it potentially suitable for high-end consumer electronics requiring advanced visual displays, such as smart watches, advanced home entertainment systems, or high-definition display panels.
- Medical Imaging: With its floating-point unit and digital signal processing capabilities, this component might be used in medical devices that require rapid and accurate processing capabilities, such as digital imaging modalities. Integration and interfacing with various sensors can be efficiently managed using its ample GPIO capabilities.
- IoT Devices: Given its connectivity features and the inclusion of Direct Memory Access (DMA) channels, the STM32F469IIT6 could be well-suited for Internet of Things (IoT) devices, which require efficient data handling and power management, which are supported by its varied supply voltage options.
It is important to note that these potential applications are conceptual and should be thoroughly analyzed by engineering and design teams to ensure compliance with industry standards and specific application needs.
About STMicroelectronics
STMicroelectronics is a global semiconductor leader delivering intelligent and energy-efficient products and solutions that power the electronics at the heart of everyday life. STMicroelectronics’ products are found everywhere today, and together with our customers, they are enabling smarter driving and smarter factories, cities and homes, along with the next generation of mobile and Internet of Things devices.
The microcontroller lineup from STMicroelectronics, especially the Microcontrollers subcategory in which STM32F469IIT6 resides, is renowned for integrating advanced chip design with a focus on catering to the robust needs of high-growth industries. The brand is known for ongoing innovation and has maintained competitive manufacturing capabilities that stand out in the semiconductor market.
Where to Find STM32F469IIT6 by STMicroelectronics
If you are considering purchasing the STM32F469IIT6, or are searching for alternative solutions, it is recommended that you visit Microcontrollers on FindChips.com. There you will find up-to-date pricing, stock levels, and datasheets directly from distributors. Historically, this part has been available from distributors like LCSC, EBV Elektronik, Mouser Electronics, and DigiKey. It’s essential to check current availability and lead times as these can vary.