TLS360™ from Rochester Electronics: Lifecycle Assurance, Without Compromise

TLS360 Rochester Electronics

A New Planning Reference for Mission-Critical Semiconductor Obsolescence

For engineers working on long-lifecycle systems such as aerospace and defense platforms, industrial controls, medical devices, and transportation infrastructure, obsolescence is a recurring, costly certainty. A part that is active today can be flagged for discontinuation years before the system it powers is scheduled to retire, forcing a familiar, expensive choice: redesign around a new component or rush to secure enough inventory to bridge the gap.

Rochester Electronics is combating obsolescence with Through Life Support 360 (TLS360), our program-level lifecycle assurance offering for select mission-critical semiconductor product families.

What is TLS360?

Standard semiconductor lifecycles are built around the original manufacturer’s roadmap. Once a part reaches end-of-life milestones, it typically transitions to “Not Recommended for New Designs” (NRND), then to formal discontinuation—regardless of how long the systems that rely on it are expected to remain in service.

TLS360 extends active status on designated parts beyond the point when they would normally begin transitioning. Because Rochester Electronics operates as a 100% authorized distributor and licensed semiconductor manufacturer for the families we cover, we can provide lifecycle assurance that supports risk-free, long-term production and a continued governed supply within the same fully authorized framework under which the part was originally shipped. For design teams, that translates into a practical benefit: existing designs can remain in production longer without forced redesigns or reactive, last-minute sourcing.

The program currently covers select design-anchor product families from manufacturers including Texas Instruments, Analog Devices, NXP, and Infineon, with additional coverage added as authorized programs expand.

A Planning Reference, not a Guessing Game

Every designated part number is assigned one of three lifecycle horizons:

  • Micro (1–3 years): Authorized inventory with near-term planning
  • Mid (4–6 years): Strategic inventory plus licensed manufacturing readiness (where authorized)
  • Max (7+ years): Long-range continuity for design-anchor families, including licensed manufacturing (where authorized)

TLS360 gives each part a defined horizon that can be built directly into a program’s planning cycle. Combined with market intelligence tools such as Findchips—which provides engineers with visibility into pricing, inventory, and lifecycle information—TLS360 helps organizations move from reactive sourcing to proactive lifecycle management. Horizons are reviewed on an ongoing basis through our formal governance process as new supplier data, inventory positions, and manufacturing status come in.

Those lifecycle horizon determinations are informed in part by agentic AI systems that analyze authorized supplier data, historical lifecycle patterns, inventory signals, and change-notification inputs. We treat this as augmentation rather than automation of decision-making. The AI-assisted analysis informs our governance process, but final lifecycle classifications remain subject to human review.

Built on Industry Terms, not a Parallel Standard

A common failure mode of proprietary lifecycle programs is that they create their own vocabulary—forcing customers to translate between “what the manufacturer says” and “what the distributor says.” TLS360 deliberately avoids this by aligning with JEDEC-defined lifecycle terminology and change-notification conventions, including standard treatment of PCNs (Product Change Notices), PDNs (Product Discontinuation Notices), and the Active/NRND/EOL progression engineers already use.

Rochester is explicit that formal PCNs and PDNs remain the authoritative lifecycle communications; TLS360’s horizons are guidance for planning purposes and are meant to be incorporated into a customer’s own risk management rather than treated as a substitute for those formal notices.

Why TLS360 Matters for Long-Lifecycle Design

For programs measured in decades rather than product cycles, the value proposition is straightforward: part-number integrity. No substitutions or forced redesigns, and consistent lifecycle treatment across related derivatives and revisions of a given device—with licensed manufacturing continuity where designated, so supply doesn’t depend solely on available inventory.

That’s a meaningful shift in how obsolescence risk is managed upstream. Instead of learning of a critical component’s discontinuation notice after the fact, design and procurement teams working with TLS360-designated parts have a defined planning horizon from the outset, turning what’s traditionally a reactive, program-threatening event into a predictable part of the design lifecycle.

TLS360: Lifecycle assurance, without compromise.

Learn more about TLS360 and current program coverage.