Overview of VL53L1CBV0FY/1 by STMicroelectronics
The VL53L1CBV0FY/1 is a time-of-flight ranging sensor that provides advanced multi-zone and multi-object detection capabilities. Designed for a wide variety of applications, this proximity sensor operates efficiently in a temperature range of -20 to 85 degrees Celsius. The device belongs to the electronic parts subcategory of Other Signal Circuits in the category of Signal Circuits, making it a versatile option for various electronic systems.
It is essential to note that as of the time of writing, this part has an active life cycle status. The VL53L1CBV0FY/1 has a package description of LGA-12, which indicates its compact design suitable for surface mount applications. The sensor comprises 12 terminals configured in a grid array format, allowing for efficient integration into various hardware systems.
This sensor is classified as compliant with RoHS and REACH regulations, ensuring that it meets environmental safety standards. It is also encoded under ECCN Code EAR99, indicating that it is subject to U.S. export control, though it does not fall under a specific dual-use category. The compliance factors make the VL53L1CBV0FY/1 an excellent choice for industries that emphasize sustainability and regulatory adherence.
In terms of manufacturing details, it boasts a factory lead time of approximately 16 weeks and 3 days, which may be significant for project timelines that require prompt delivery. The peak reflow temperature and associated thermal management details have not been specified, ensuring that design engineers should account for their own thermal considerations when integrating this sensor into systems.
Industry Applications for VL53L1CBV0FY/1
The VL53L1CBV0FY/1 proximity sensor might find potential use cases across various industries. Here are some areas where this component could be particularly beneficial:
- Internet of Things (IoT): The VL53L1CBV0FY/1 could be integrated into smart home devices, enabling features such as gesture recognition or presence sensing. It could help optimize energy consumption by detecting occupancy in rooms, which could lead to energy-efficient designs.
- Transportation and Logistics: In autonomous vehicles or logistics tracking solutions, this sensor might be used for distance measurement and obstacle avoidance. The advanced multi-object detection capability could help improve situational awareness in crowded environments, possibly enhancing safety and efficiency.
- Consumer Electronics: This sensor could be employed in mobile devices for proximity sensing, enabling features such as auto-screen-off during calls. Similarly, it could enhance user interaction in augmented reality (AR) or virtual reality (VR) applications by accurately tracking user movements.
- Robotics and Drones: The VL53L1CBV0FY/1 could potentially be utilized in robotic navigation systems, enabling robots to detect objects and navigate through complex environments. Its multi-zone detection capability may allow for more sophisticated movement and obstacle avoidance techniques.
- Security and Surveillance: This sensor might be used in security systems for motion detection, allowing for better monitoring of premises. The ability to detect multiple zones could help create more detailed surveillance coverage and increase the effectiveness of security protocols.
These potential industry applications are strictly conceptual and illustrative. Engineering and design teams should conduct thorough analysis and verification processes to ensure adherence to industry standards and specific application requirements. Further studies may also reveal how similar parts in this category could be effective for these applications as well.
About STMicroelectronics
STMicroelectronics is a leading manufacturer in the semiconductor industry, particularly recognized for its comprehensive portfolio of products, including those in the category of Other Signal Circuits. The company’s commitment to innovation and quality has made it a major player in various sectors, including automotive, industrial, and consumer electronics.
The VL53L1CBV0FY/1 is just one of several time-of-flight sensors that STMicroelectronics offers, which demonstrates their expertise in developing technologies that address the growing needs for more precise and efficient detection and ranging solutions. STMicroelectronics also manufactures several similar parts, which share common features and specifications, allowing design engineers to select the appropriate sensor that meets their specific application requirements.
Where to Find VL53L1CBV0FY/1 by STMicroelectronics
Historically, the VL53L1CBV0FY/1 has been available through a variety of distributors, including:
- Avnet Americas
- Future Electronics
- DigiKey
- Mouser Electronics
While these distributors have previously stocked this part, it is crucial to check findchips.com for the most current availability and pricing.