Overview of 1EDN7512GXTMA1 by Infineon Technologies AG
The 1EDN7512GXTMA1 is characterized as a half-bridge based MOSFET driver with a package type of PDSO6, specifically in a WSON-6 form factor. Originating from Infineon Technologies AG, this component is designed to operate within a temperature range of -40 to 150°C, offering a low-side driver configuration. It boasts a peak output current of 8A and supports a supply voltage ranging from 4.5V to a maximum of 20V. The driver is housed in a WSON, driver case style, comprising 6 pins in total.
Regarding timing, both the input and output delays are marked at 19ns, providing swift signal transitions that benefit applications requiring rapid response times. Notably, this part is also compliant with RoHS standards, emphasizing its suitability for use in environmentally sensitive applications. Given its specifications, including a moisture sensitivity level (MSL) of 1, the 1EDN7512GXTMA1 is designed for robust performance in a variety of challenging environments.
Industry Applications for 1EDN7512GXTMA1
The 1EDN7512GXTMA1, attributable to its versatility and performance characteristics, finds its utility across a broad spectrum of industry applications. Here are some potential applications, underlining the need for thorough validation by design and engineering teams:
- Industrial Automation: In automation applications, this driver could potentially be used to control high-speed gates in power electronics, contributing to more efficient machinery operation or in protective circuits.
- Energy and Power Systems: Its robust design and capability to handle significant power levels make it suitable for applications in power conversion systems, such as inverters and power regulators used within energy production and distribution infrastructures.
- Renewable Energy Systems: The 1EDN7512GXTMA1 could find applications in solar inverters or wind turbine converters, where efficient and reliable low-side driving is crucial for energy harvesting and conversion.
- Automotive: Within the automotive sector, this part might be utilized in electric vehicle (EV) charging stations, powertrain modules, or in the control units of hybrid/electric vehicles, where high reliability and efficiency are paramount.
It’s vital to note that these possible applications should require meticulous analysis and verification by engineering and design teams to ensure the part fulfills the specific requirements of the intended use case.
About Infineon Technologies AG
Infineon Technologies AG stands as a pivotal manufacturer in the realms of MOSFET Drivers and Drivers And Interfaces at large. Their commitment to innovation, quality, and sustainability has positioned them as a leader in semiconductor solutions, providing a wide array of electronic components that serve various sectors including automotive, industrial, IoT, and consumer electronics. The 1EDN7512GXTMA1 is just one example of Infineon’s dedication to developing high-performance and durable products. Infineon is known for its extensive portfolio of MOSFET drivers, which are designed to meet diverse application requirements, offering both high-side and low-side driving solutions that ensure reliable operation in demanding environments.
Where to Find 1EDN7512GXTMA1 by Infineon Technologies AG
To procure the 1EDN7512GXTMA1, it is advisable to conduct thorough research starting with findchips.com. This platform allows for the comparison of stock levels and pricing among various distributors. Historically, distributors such as EBV Elektronik, Ameya Holding Limited, Rochester Electronics, Bristol Electronics, Future Electronics, Mouser Electronics, Avnet Americas, DigiKey, and Newark have been known to stock this particular part. However, availability can fluctuate, emphasizing the importance of using findchips.com to obtain the most current availability and pricing information. Additionally, for those seeking alternatives to the 1EDN7512GXTMA1 or exploring other Infineon Technologies AG offerings, the MOSFET Drivers category on findchips.com can serve as a valuable resource for comparable components from Infineon or other manufacturers.