AA4040P3C-P22 by Kingbright

Overview of AA4040P3C-P22 by Kingbright

The AA4040P3C-P22 is a photo transistor specifically designed for optical sensing applications. It operates at a wavelength of 940 nm and features a side view SMD (Surface Mount Device) configuration, making it suitable for various compact electronic designs. With a size of 4×4 mm, this component is optimized for space-sensitive applications while providing reliable performance. Manufactured by Kingbright Electronic Co Ltd, the component is actively supported in the market, reinforcing its availability for project designers and engineers.

In terms of compliance, the AA4040P3C-P22 adheres to RoHS (Restriction of Hazardous Substances) standards, ensuring that it is free from hazardous materials that could pose a risk to health and the environment. Additionally, the part meets REACH (Registration, Evaluation, Authorisation and Restriction of Chemicals) compliance requirements. As of the current writing, the part is listed as active in Kingbright’s product lineup, indicating ongoing production and support for this device.

Industry Applications for AA4040P3C-P22

The versatility of the AA4040P3C-P22 photo transistor makes it suitable for a variety of industries, including but not limited to the following examples:

  • Internet of Things (IoT): The AA4040P3C-P22 might be utilized in smart home devices, where it could serve as a sensor for motion detection or light level sensing. Its compact size and side view configuration allow for unobtrusive placement within various devices.
  • Environmental Monitoring: This photo transistor could potentially be part of environmental sensors that measure air quality or light pollution, providing real-time data to connected systems for analysis and reporting.
  • Smart Cities: In smart city applications, the AA4040P3C-P22 might be integrated into systems for traffic monitoring, pedestrian detection, or waste management alerts. Its optical sensing capabilities can facilitate automated responses to environmental changes.
  • Robotics and Drones: The component could be useful in robotic systems that require object detection or obstacle avoidance. Its rapid sensing response might enhance the safety and operational efficiency of drones or autonomous vehicles.
  • Consumer Electronics: In consumer electronics, the AA4040P3C-P22 might be found in devices such as cameras or smartphones, where it could assist with automatic brightness adjustments or gesture recognition.

Note that these potential industry applications are only conceptual and illustrative. Design and engineering teams must analyze and verify that the AA4040P3C-P22 adheres to industry standards and specific application requirements before implementation.

About Kingbright

Kingbright is a manufacturer recognized within the optoelectronics sector, specializing in various types of optoelectronic devices, including displays, LEDs, and phototransistors. The company has a history of producing reliable components such as the AA4040P3C-P22, which are characterized by their high performance and compliance with international standards. Kingbright’s focus on innovation and quality ensures that their products, including those in the photo transistor category, meet the diverse needs of industries ranging from consumer electronics to industrial automation.

In addition to the AA4040P3C-P22, Kingbright also manufactures similar parts that fall within the same category, providing engineers with a range of options to suit different project requirements. Their commitment to high-quality production ensures continued use across a variety of applications.

Research Price and Stock for AA4040P3C-P22 by Kingbright on Findchips.com

For those interested in procuring the AA4040P3C-P22, it is advisable to conduct research on stock levels and pricing through Findchips. This resource provides an efficient way to compare offerings from various distributors. Historically, the part has been available through distributors such as Sager, TTI, Future Electronics, Mouser Electronics, and DigiKey. However, stock levels may vary, so it is essential to check Findchips for the most current information.

Additionally, the site allows users to explore alternate parts within the Photo Transistors subcategory, which might also include comparable offerings from Kingbright or other manufacturers. This can be particularly useful for engineers seeking alternatives or replacements in their designs.

Compare pricing for AA4040P3C-P22 and other Photo Transistors / Optoelectronics at findchips.com