Overview of STM32WL55JCI6 by STMicroelectronics
The STM32WL55JCI6 is a dual-core microcontroller that integrates both an Arm Cortex-M4 and an Arm Cortex-M0+ processor, operating at a frequency of 48 MHz. It is classified as a Sub-GHz Wireless Microcontroller, specifically designed to enhance communication capabilities in various applications. The part comes equipped with 256 Kbytes of Flash memory and 64 Kbytes of SRAM, making it suitable for a range of applications that require processing power and memory to handle complex tasks.
This microcontroller supports multiple modulations, including LoRa, (G)FSK, (G)MSK, and BPSK, allowing for versatile wireless communication solutions. The inclusion of AES 256-bit encryption adds a layer of security for applications where data integrity and confidentiality are paramount. The subcategory of Microcontrollers refers to its classification within the broader category of Microcontrollers and Processors, highlighting its role as an essential component in embedded systems.
Furthermore, the STM32WL55JCI6 is presented in a UFBGA-73 package and complies with ROHS standards, ensuring adherence to environmental regulations. As of this writing, the factory lead time for this part is approximately 16 weeks and 4 days, making it important for planning and inventory management in procurement processes.
Industry Applications for STM32WL55JCI6
The versatility of the STM32WL55JCI6 microcontroller lends itself to a variety of potential industry applications. Below are some example industries and how this component might be utilized within them:
- Internet of Things (IoT): The STM32WL55JCI6 could serve as a core component in various IoT devices such as smart home sensors or connected appliances. With its sub-GHz wireless capabilities and encryption features, it might facilitate secure communication between devices while processing data locally.
- Environmental Monitoring: This microcontroller could potentially be used in applications like smart weather stations or pollution sensors. Its capacity for LoRa communication might allow for long-range data transmission, making it suitable for remote environmental monitoring.
- Smart Cities: The technology could find usage in smart city applications such as public lighting systems or smart waste management solutions. Its ability to support various wireless protocols might optimize communication in urban infrastructure.
- Telecommunications: Within telecommunication systems, the STM32WL55JCI6 could potentially be implemented in base stations or sensor networks, enabling efficient communication through its multiprotocol capabilities.
- Consumer Electronics: The part might also be found in consumer electronic devices, such as wireless audio systems or remote controls, where low power consumption and wireless performance are critical.
It is important to note that these potential industry applications are conceptual and illustrative in nature. They require thorough analysis and verification by engineering and design teams to ensure compliance with industry standards and specific application requirements.
About STMicroelectronics
STMicroelectronics is a global leader in providing semiconductor solutions, particularly in the realm of Microcontrollers and Processors. The company has a strong focus on developing innovative technologies, consistently working to enhance performance while minimizing power consumption. The STM32WL55JCI6 is a notable example of their STM32 family, which features a range of microcontrollers designed to cater to diverse application needs.
In addition to the STM32WL55JCI6, STMicroelectronics manufactures a variety of similar parts that support wireless communication, including those within the STM32W series. This provides engineers and designers multiple options to select from, based on their specific requirements for processing power, memory, and communication features.
Research Price and Stock for STM32WL55JCI6 by STMicroelectronics on Findchips.com
For those seeking to procure the STM32WL55JCI6, it is recommended to research current stock levels and pricing on Findchips. This platform is a valuable resource for exploring availability from various distributors. Historical availability records indicate that distributors such as EBV Elektronik, Avnet Silica, Future Electronics, STMicroelectronics, Mouser Electronics, DigiKey, and Newark have previously offered this part. However, users should consult Findchips to verify current stock status and pricing.