Overview of BTS70802EPAXUMA1 by Infineon Technologies AG
The BTS70802EPAXUMA1 is a buffer/inverter-based peripheral driver that features a range of specifications suitable for various applications. Designed for high side switching, this component has an input voltage threshold of 28V, making it adept at managing significant power loads. With a current limit set at 36A and a maximum output current of 3A, the BTS70802EPAXUMA1 is capable of handling substantial current without compromising performance.
Manufactured in a TSSOP-14 package style with 14 pins, the part also boasts a low on-state resistance of 0.0209 ohm, which can enhance efficiency by minimizing power loss. The operational characteristics are further bolstered by built-in protections against transient events, overcurrent conditions, overvoltage scenarios, and thermal issues. As of the current writing, the factory lead time for this product is observed to be around 20 weeks, which is a critical factor for procurement and manufacturing scheduling.
Industry Applications for BTS70802EPAXUMA1
The versatility of the BTS70802EPAXUMA1 makes it potentially applicable in various industries. Here are a few examples of how this part could be utilized:
- Industrial Automation: In applications where high current needs are common, such as in control systems for motors or actuators, the BTS70802EPAXUMA1 might serve as a crucial component in the driving circuitry. Its rapid turn-on and turn-off times (110 µs and 100 µs, respectively) could aid in effective control of these devices.
- Smart Cities: This part could potentially find use in smarter infrastructure systems, such as automated street lighting and traffic management systems. Its ability to handle high current loads might facilitate the effective powering of LED arrays or signal systems.
- Automotive Applications: Given its compliance with AEC-Q100 standards, the BTS70802EPAXUMA1 might be ideal for automotive applications such as power management systems within electric and hybrid vehicles. The built-in thermal protection feature could provide extra reliability in demanding environments.
- Consumer Electronics: The part may also be utilized in devices demanding efficient power management, such as laptops or gaming consoles. Its low on-state resistance could contribute to energy-saving features in these devices.
- Robotics and Drones: The BTS70802EPAXUMA1 might be integrated into the control circuits of drones or robotic systems where precise and rapid switching of power loads is necessary for operations or movements.
These potential industry applications are only conceptual and illustrative. It is essential for engineering and design teams to conduct thorough analyses and verifications to ensure adherence to industry standards and specific application requirements.
About Infineon Technologies AG
Infineon Technologies AG is a manufacturer with a robust portfolio in the electronic component market, particularly focusing on drivers and interfaces. The company is known for its commitment to innovation and quality, especially in the realm of peripheral drivers such as the BTS70802EPAXUMA1. Infineon also produces several other similar parts designed to manage high current loads and provide integral protection features, supporting a wide range of applications across multiple industries.
The manufacturer’s focus on AEC-Q100 compliance for automotive applications is particularly significant, as this standard ensures reliability in environments subject to vibration, temperature extremes, and other demanding conditions. Infineon Technologies AG continues to expand its offerings in the area of peripheral drivers, which serve as critical components in modern electronic systems.
Research Price and Stock for BTS70802EPAXUMA1 by Infineon Technologies AG on Findchips.com
For those interested in acquiring the BTS70802EPAXUMA1, it is recommended to research current stock and pricing at Findchips.com. This platform provides valuable insights into availability and cost, allowing procurement teams to make informed decisions.
Historically, this part has been available from a range of distributors, including:
- Win Source Electronics
- EBV Elektronik
- Chip One Stop
- TME
- Rochester Electronics
- Future Electronics
- Mouser Electronics
- Avnet Americas
- DigiKey
- Newark
However, current stock levels and pricing may vary, so checking Findchips for the latest information is crucial to ensure timely procurement.