Overview of MAX30003CWV+T by Analog Devices Inc.
The MAX30003CWV+T by Analog Devices Inc. is an ultra-low power, single-channel integrated biopotential analog front end (AFE) designed specifically for electrocardiogram (ECG) and R to R detection applications. Packaged in a 30-pin, very thin profile fine pitch ball grid array (VFBGA), this component measures only 2.926 by 2.74 mm, making it ideally suited for compact medical and healthcare devices where space is at a premium.
This part falls under the category of Other Signal Circuits and is notable for its low supply voltage range, functioning between 1.1 V and 2 V, with a nominal voltage of 1.8 V. It features a CMOS technology base, which provides an efficient operation in terms of power consumption, critical for battery-operated or portable applications. The device was introduced into the market on June 29, 2016, indicating its relatively recent development and adoption in modern circuits.
The MAX30003CWV+T is built to accommodate commercial temperature grades (0 to 70°C) and has a peak reflow temperature of 260°C, tolerable for most standard assembly processes. It comes with a moisture sensitivity level of 1, which denotes that it needs very minimal protection from moisture, beneficial in reducing packaging and handling costs.
Industry Applications for MAX30003CWV+T
The specific design and technical attributes of MAX30003CWV+T make it ideally suited for several potential applications, particularly in fields requiring precise and reliable monitoring of bioelectrical signals. Here, we explore some key industries:
- Healthcare: The component’s primary design for ECG applications means it could be crucial in developing wearable health monitoring devices that require long battery life and compact size. Devices such as personal heart rate monitors or event monitors, which provide ongoing observation of patients, could benefit significantly from this AFE’s capabilities.
- Medical Imaging: While traditionally used for ECG, the applications of MAX30003CWV+T can extend to more complex medical imaging technologies where biopotential measurements are critical. This might include certain types of biofeedback therapy devices, where understanding the electrical signals of the body can help tailor therapeutic responses.
- Environmental Monitoring: In contexts where bioelectrical data can contribute to environmental studies, such as studies on physiological responses to environmental stresses, the MAX30003CWV+T can provide the necessary data analysis tools for field researchers.
Note: The potential industry applications listed are conceptual and should be further evaluated by engineering and design teams for compliance with relevant industry standards and requirements specific to actual use cases.
About Analog Devices Inc.
Analog Devices Inc. is a prestigious player in the realm of electronic components, specifically known for their robust range of signal processing technologies. This company excels in integrating physical world phenomena into digital insights, making them a vital contributor to the Other Signal Circuits category.
One of their notable parts, the MAX30003CWV+T, exemplifies their commitment to advancing the capabilities and applications of bioelectronic devices. Analog Devices Inc. consistently pushes for innovation in this area, creating components that enhance the accuracy and function of devices in medical and health applications.
Where to Find MAX30003CWV+T by Analog Devices Inc
To purchase the MAX30003CWV+T, it’s recommended that interested buyers utilize findchips.com. This platform provides the most current stock levels and competitive pricing from various distributors. Historically, this part has been available from distributors such as Chip1Stop, Analog Devices Inc, and Mouser Electronics. Visit Other Signal Circuits to find alternate parts by Analog Devices Inc or other manufacturers.