MPU-6500 by InvenSense Inc

Overview of MPU-6500 by InvenSense Inc.

The MPU-6500 by InvenSense Inc. is an integrated 6-axis MotionTracking device, combining a 3-axis gyroscope and a 3-axis accelerometer. It is encapsulated in a 3 x 3 mm, 0.90 mm height, green, QFN-24 package. Manufactured using CMOS technology, it’s designed for low-power, low-voltage applications, making it an ideal choice for portable electronics. It operates across a wide range of temperatures, from -40°C to 85°C, meeting the industrial temperature grade requirements. This other signal circuits component is designed for seamless integration into various electronic projects, owing to its small form factor and high performance.

Key characteristics include a nominal supply voltage of 1.8 V, with a broad range from 1.71 V to 3.45 V, accommodating various power supply designs. It supports I2C communication, enabling easy interfacing with most microcontrollers and digital systems. The MPU-6500’s packaging and terminal finishes are designed for reliability and robust performance in diverse applications. With RoHS compliance, it meets global environmental standards, ensuring suitability for a wide range of applications in environmentally sensitive markets.

Industry Applications for MPU-6500

The MPU-6500’s versatile feature set makes it well-suited for a broad array of industry applications. While it directly aligns with fields like consumer electronics, Internet of Things (IoT), robotics, and drones, its potential use cases expand much further. The following applications provide a glimpse into how the MPU-6500 could be integrated into various industries, emphasizing that these scenarios should be further investigated for compatibility and meeting specific requirements.

  • Wearable Technology: In the domain of consumer electronics, especially wearable devices, this component might serve as a pivotal sensor for motion tracking and activity recognition. Its low power consumption and small footprint could be especially advantageous in compact devices like smartwatches, fitness trackers, and virtual reality headsets, where space and power efficiency are paramount.
  • Automated Industrial Systems: Within IoT applications, the MPU-6500 could potentially be crucial for industrial automation systems where precision motion sensing is required. Examples include robotic arms and automated guided vehicles (AGVs), where accurate motion data can optimize performance and efficiency.
  • Smart Home Devices: The agility and efficiency of this component might also make it suitable for smart home applications. Devices such as robotic vacuum cleaners and smart home security systems that require environmental interaction and navigation could benefit from its precise motion tracking capabilities.
  • Academic Research and Development: In research contexts, particularly those focused on motion detection and analysis, the MPU-6500 could be instrumental. University projects and commercial R&D labs focusing on new robotics and drone technologies could leverage this sensor for various experimental and development purposes, given its robust performance and versatile application potential.

It is crucial to note that these potential industry applications are conceptual and need thorough analysis and verification by engineering and design teams to ensure compliance with specific standards and requirements.

About InvenSense Inc.

InvenSense Inc., a leading entity in the realm of motion sensor solutions, has carved a niche in the production of MEMS (Micro-Electro-Mechanical Systems) based sensors. Their expertise lies broadly within the signal circuits realm, including significant contributions to other signal circuits. The MPU-6500 is a testament to InvenSense’s commitment to innovation and quality in the design and manufacture of sophisticated motion tracking devices.

InvenSense’s sensors are pivotal for a multitude of applications ranging from mobile and wearable devices to automotive and industrial equipment. Recognizing the increasing demand for high-performance, reliable, and cost-effective motion tracking devices, InvenSenses continually expands its product portfolio to meet and exceed market expectations. The company’s dedication to quality, performance, and support has established its products as go-to solutions for engineers and designers across various sectors.

Where to Find MPU-6500 by InvenSense Inc

For those looking to procure the MPU-6500, findchips.com offers a comprehensive platform to check current stock levels, pricing, and distributor availability. While the part has historically been available at distributors like Win Source Electronics, LCSC, Avnet Abacus, and DigiKey, it is essential to visit findchips.com to obtain the latest information regarding availability and pricing. Additionally, for projects that might require alternative or similar components, the Other Signal Circuits section provides a diverse selection from InvenSense Inc. and other manufacturers, enabling designers to find the perfect match for their specific application needs.

Compare pricing for MPU-6500 and other Other Signal Circuits / Signal Circuits at findchips.com