RT0W01419PNH03 by Amphenol Corporation

Overview of RT0W01419PNH03 by Amphenol Corporation

The RT0W01419PNH03 is a standard circular connector designed specifically as a receptacle featuring a square flange. This connector is characterized by its 19 positions and male configuration, with a shell size of 14. The part also includes a silicone seal, which enhances its durability and resistance to environmental conditions. The use of silicone seals contributes to the reliability of the connection by providing protection against dust, moisture, and other contaminants that might interfere with performance over time.

Manufactured by Amphenol Corporation, a recognized leader in the manufacturing of electronic connectors, the RT0W01419PNH03 fits within the subcategory of Other Circular Connectors. This part is part of the active life cycle code, signaling its availability and ongoing production. The RoHS (Restriction of Hazardous Substances) compliance indicates that the part meets environmental and safety standards set to minimize harmful substances in electronic products. The part also adheres to REACH compliance, assuring that it meets European legislation for chemical safety.

Industry Applications for RT0W01419PNH03

The potential applications for the RT0W01419PNH03 can be considered across various industries that rely on robust and reliable connections. Below are some example sector applications:

  • Industrial Automation: In industrial settings, this connector might serve in machinery and equipment where durable connections are essential, such as in robotics or process automation. The silicone seal could provide enhanced protection against industrial spills and contaminants.
  • Aerospace and Defense: The characteristics of the RT0W01419PNH03 might make it suitable for applications in aerospace systems that require connectors capable of withstanding extreme conditions. Its square flange design could facilitate secure mounting in complex assemblies.
  • Telecommunications: This connector may find use in telecommunications equipment, where reliable connections are critical for maintaining communication networks. The 19 positions could allow for multiple connections within a singular housing, streamlining connectivity solutions.
  • Transportation and Logistics: In this sector, connectors like the RT0W01419PNH03 might be utilized in various transport systems, ensuring that electronic systems in vehicles and logistics equipment are effectively interconnected.
  • Consumer Electronics: The robust nature of this connector could see it applied in consumer electronics, where an effective and durable connection is necessary for device functionality and user safety.

These potential industry applications are only conceptual and illustrative and require thorough analysis and verification by engineering and design teams to ensure adherence to industry standards and specific application requirements. Similar connectors might also be employed in these applications for enhanced versatility based on the unique demands of each project.

About Amphenol Corporation

Amphenol Corporation stands as a significant entity in the connector manufacturing domain, particularly known for producing a broad array of connectors, including Other Circular Connectors. The company has a legacy of delivering reliable products designed to meet diverse market needs, ensuring compatibility across a wide range of applications. The RT0W01419PNH03 is indicative of the company’s commitment to innovation and quality in the electronic components sector. Amphenol also manufactures various similar parts that might appeal to different industries, making it a valuable manufacturer for procurement teams considering options for their projects.

Where to Find RT0W01419PNH03 by Amphenol Corporation

RT0W01419PNH03, it is advisable to research the current market availability on findchips.com. This platform provides a comprehensive view of where the part can be sourced. Additionally, it offers insights into other parts within the Other Circular Connectors category that may meet similar requirements. Previously, this part has been available through distributors such as Avnet Americas and Mouser Electronics, although current stock levels and pricing should be confirmed directly on findchips.com to ensure availability.

Compare pricing for RT0W01419PNH03 and other Other Circular Connectors / Connectors at findchips.com