STM32H743XIH6 by STMicroelectronics

Overview of STM32H743XIH6 by STMicroelectronics

The STM32H743XIH6 by STMicroelectronics is a cutting-edge Microcontroller integrated with a broad set of features tailored for high-performance applications. This device integrates a high-performance ARM Cortex-M7 processor capable of running up to 480 MHz. It is equipped with 2MB of Flash memory and 1MB of RAM, providing ample storage and processing capabilities for complex operations. The inclusion of a Digital Signal Processor (DSP) and a Double-Precision Floating Point Unit (DP-FPU) enhances its capacity for scientific calculations and real-time data processing.

STMicroelectronics has designed the STM32H743XIH6 with a comprehensive set of peripherals including advanced control timers, a real-time clock, SAI (Serial Audio Interface), SDMMC (Secure Digital Memory Card interface), and USB OTG (On-The-Go). Additionally, its external memory interface facilitates expanded storage and memory options for broader application utility. The device is packaged in a TFBGA-265 (Thin-Fine Ball Grid Array), providing a compact form factor suitable for high-density board designs. Given its broad operating voltage range from 1.62V to 3.6V, the STM32H743XIH6 is versatile for a wide range of power scenarios.

Industry Applications for STM32H743XIH6

The STM32H743XIH6, with its robust feature set, finds usage across a diverse spectrum of industries. Here are a few applications where its high performance, connectivity options, and processing power could be particularly beneficial:

  • Internet of Things (IoT): Its advanced features enable smart connectivity solutions in homes, industrial automation, and smart city infrastructure, potentially connecting hundreds of sensors over complex networks.
  • Consumer Electronics: Products such as wearable technology, high-performance drones, and advanced personal assistants could utilize the STM32H743XIH6 for its processing capabilities and low power consumption.
  • Transportation and Logistics: Vehicle tracking systems, advanced navigation controls, and fleet management solutions could benefit from the extensive I/O capabilities and robust processing power.
  • Medical Devices: microcontrollers similar to the STM32H743XIH6 might be considered for applications in healthcare technologies, where precision, reliability, and computational capabilities are paramount. Devices such as portable heart monitors and advanced diagnostic systems could potentially incorporate this MCU, assuming it passes evaluation for industry and regulatory requirements.

It’s important to highlight that these potential applications are conceptual and illustrative, depending on specific requirements and considerations. Engineering and design teams need to conduct thorough analysis and verification before selecting this or any component for a project.

About STMicroelectronics

STMicroelectronics is a global leader in the semiconductor industry, providing a broad array of electronic components related to Microcontrollers and Processors, among other categories. The company is renowned for its innovation in the semiconductor space, offering products that serve a myriad of applications from automotive to industrial and beyond. STMicroelectronics has established a solid reputation for quality, reliability, and advancement in technology, particularly noted in its wide range of microcontrollers.

The STM32H743XIH6 is part of the STM32 family, which is known for its high performance, flexibility, and efficiency, serving as a backbone for many modern electronic devices. STMicroelectronics continuously invests in research and development to push the boundaries of what its products can achieve, ensuring they meet the growing demands of the technology landscape.

Where to Find STM32H743XIH6 by STMicroelectronics

To find the STM32H743XIH6, your best resource is findchips.com. This site offers comprehensive search tools to compare stock levels and pricing across a wide range of distributors. Traditionally, the part has been available from several distributors, including Ameya Holding Limited, TME, Future Electronics, STMicroelectronics Direct, Mouser Electronics, Avnet Americas, and DigiKey. However, for the most current availability and best pricing information, it is crucial to research the part on FindChips.

For those exploring alternatives or looking for parts with similar functionalities, FindChips offers a robust database of Microcontrollers that might be offered by STMicroelectronics or other leading manufacturers.

Compare pricing for STM32H743XIH6 and other Microcontrollers / Microcontrollers and Processors at findchips.com