Overview of 0804293:0001 by Phoenix Contact
The 0804293:0001 by Phoenix Contact is a terminal block accessory specifically designed for marking, identified as a marking item. The specific model, Sk 5 08/3 8: Fortl.zahlen 1-10, features a marker card printed with numbers 1-10, facilitating the organization and identification in wiring applications. As part of the Assembly Items subcategory under Connector Support, this component ensures enhanced clarity and efficiency in electrical panel setups.
Phoenix Contact, a reputable entity in the manufacturing of electrical connection, electronic interface, and industrial automation technologies, promotes this part as RoHS compliant, indicating its manufacturing adherence to restrictive hazardous materials standards, essential for ensuring environmental safety and end-user health.
Industry Applications for 0804293:0001
The marker card 0804293:0001 is stipulated for usage across multiple industries depending on the specific needs for system organization and clarity in terminal block applications. Potential industry use cases for this part are conceptual and require further validation:
- Industrial Automation: In this sector, organization and clarity in control panels and power distribution units are crucial. The 0804293:0001 could potentially facilitate the identification of connections, leading to faster maintenance operations and reduced downtime.
- Telecommunications: With expansive networks relying on precise cabling and setups, effective marking items such as 0804293:0001 potentially aid in identifying crucial junctions and connections, possibly reducing errors during system expansions or troubleshooting.
- Consumer Electronics: In the manufacturing stages of home appliances and consumer electronics that require intricate wiring systems, clear and precise marking may help in ensuring accurate assembly and quality control.
- Aerospace and Defense: Although not specifically rated for military standards as per its attributes, in non-critical applications within these sectors where efficient identification of electrical components is crucial, such marking tools might still find limited application.
Note that these potential industry applications are illustrative and require thorough analysis and verification by engineering and design teams for adherence to specific industry standards and application requirements.
About Phoenix Contact
Phoenix Contact is a leader in the field of electrical engineering and automation, specializing in the manufacturing of innovative products for electrical connections and industrial automation applications. The company’s offerings within Assembly Items, including the 0804293:0001, address essential needs in various fields, facilitating better connectivity and system functionalities. Phoenix Contact’s commitment to quality and sustainability is reflected in their production practices, ensuring their products like the 0804293:0001 comply with important environmental standards such as RoHS.
Where to Find 0804293:0001 by Phoenix Contact
To purchase the 0804293:0001 or to research similar assembly items by Phoenix Contact and other manufacturers, one should visit parts like Assembly Items. This platform allows users to verify current stock levels and compare pricing across multiple distributors. Previously, this part has been listed at distributors such as Neutron USA, Master Electronics, Dynamic Solutions GmbH, Sager, Onlinecomponents.com, Mouser Electronics, DigiKey, and Newark. However, to get the most current availability and pricing, checking Findchips.com is recommended.