D12V0H1U2LP-7B by Diodes Incorporated

Overview of D12V0H1U2LP-7B by Diodes Incorporated

The D12V0H1U2LP-7B is a Transient Voltage Suppressor Diode characterized by its unidirectional configuration, with an operational peak reverse voltage of 12V and a clamping voltage maximum of 23V. This makes it an effective solution for protecting circuits by shunting excessive voltage caused by transients away from sensitive components. The diode is designed using silicon technology and is encapsulated in a small, lead-free X1-DFN1006-2 package, which features two terminals.

Manufactured by Diodes Incorporated, this component promises durability and performance in demanding applications, confirmed by its compliance with RoHS and its classification under the JEDEC JESD-30 standard as a plastic, rectangular-shaped chip carrier. Furthermore, the D12V0H1U2LP-7B operates within a broad temperature range of -55°C to 150°C and has a maximum power dissipation capacity of 0.25W, aligning with the requirements of various sophisticated electronic setups.

Industry Applications for D12V0H1U2LP-7B

Given its electrical characteristics and package design, the D12V0H1U2LP-7B can potentially be utilized in a variety of industries where robust protection against voltage transients is necessary. The following sections explore possible applications within selected industries, emphasizing the conditional nature of these suggestions:

  • Consumer Electronics: Devices such as smartphones, tablets, and laptops might benefit from the integration of the D12V0H1U2LP-7B to protect sensitive digital components from electrostatic discharges (ESD) and other voltage spikes. The component’s high breakdown voltage and fast response time could be crucial in these applications.
  • Internet of Things (IoT): IoT devices, which often operate in unpredictable environments and are susceptible to various electrical disturbances, could utilize this diode for protection. The compact footprint of the D12V0H1U2LP-7B makes it suitable for space-constrained IoT devices such as sensors and smart meters.
  • Aerospace and Defense: Although specific military or aerospace standards such as MIL-spec aren’t directly mentioned for D12V0H1U2LP-7B, similar devices from Diodes Incorporated or others that meet those criteria could be used for protecting communication equipment and navigation devices against transient voltages.
  • Robotics and Drones: In robotics and drones, the D12V0H1U2LP-7B could potentially safeguard delicate circuitry from sudden voltage changes. Its ability to operate over a wide temperature range might be beneficial for outdoor robotic applications and drones flying at different altitudes.

Note: The potential industry applications suggested above are strictly conceptual and should be analyzed and verified by engineering and design teams to ensure they meet industry standards and specific requirements for each application.

About Diodes Incorporated

Diodes Incorporated is known for its comprehensive range of diodes and rectifiers, including a variety of Transient Suppressors. The company has carved a niche in the development of protection devices like the D12V0H1U2LP-7B. Their suppressors are typically designed to provide robust protection against voltage spikes and surges, and are utilized across diverse applications in the electronics industry.

With a focus on innovation and reliability, Diodes Incorporated continues to expand its offerings in this category, addressing the needs of both modern and traditional electronics. The use of advanced technologies and materials in their products ensures compliance with international safety and performance standards, making their components suitable for a global market.

Where to Find D12V0H1U2LP-7B by Diodes Incorporated

To purchase the D12V0H1U2LP-7B, a prospective buyer should start their search on findchips.com. Here, you can also explore other Transient Suppressors that might be offered by Diodes Incorporated or other manufacturers. Although this part has been available at distributors like LCSC, Avnet, Mouser Electronics, and DigiKey, checking on findchips.com will provide current stock levels and pricing, undoubtedly the most accurate and timely resource for purchasing electronic components.

Compare pricing for D12V0H1U2LP-7B and other Transient Suppressors / Diodes at findchips.com