Overview of JANTX2N2369AUB by Microchip Technology Inc.
The JANTX2N2369AUB is a small signal bipolar transistor designed primarily for switching applications. It is an NPN type silicon transistor with a breakdown voltage (V(BR)CEO) of 20 volts, making it suitable for various low-power applications. The part belongs to the electronic subcategory of small signal bipolar transistors, which are essential components in many electronic circuits for signal amplification and switching.
Microchip Technology Inc. manufactures this part, ensuring it meets various industry standards and quality requirements. The device is actively produced and is part of a broader portfolio of transistors that Microchip offers. It is worth noting that the part is not marked as ROHS compliant, which may be a consideration for some applications. Additionally, it follows the ECCN code EAR99, indicating that it is subject to U.S. export controls. The terminal finish is specified as tin-lead, which is also relevant for assembly processes and soldering compatibility.
As of this writing, the factory lead time is stated to be 22 weeks, indicating the time frame one might expect for order fulfillment. However, this timeframe is subject to change based on manufacturing demand and supply chain dynamics.
Industry Applications for JANTX2N2369AUB
The applications for JANTX2N2369AUB might span several industries, reflecting its versatility as a small signal transistor. Below are some indicative use cases where this component could potentially be integrated:
- Telecommunications: The JANTX2N2369AUB might be utilized in signal processing circuits, aiding in the amplification of low-level signals in devices such as RF amplifiers, modulators, or demodulators. Its switching capabilities could also provide key functions in telecommunications infrastructure.
- Automotive Electronics: If compliant with industry standards, the JANTX2N2369AUB could potentially be part of automotive control systems, such as in power distribution modules or sensors. Its robust design for low voltage applications could assist in various automotive functions, particularly in enhancing reliability under varying conditions.
- Consumer Electronics: This part might find applications in consumer electronic devices, such as audio amplifiers or power supply circuits, where efficient switching and amplification are crucial. Its small signal characteristics could support features that enhance the user experience in devices like televisions or audio systems.
- Industrial Automation: In this sector, the JANTX2N2369AUB might be employed in automation machinery control systems, potentially acting as a relay in low-power actuation circuits. Its ability to handle small signal switching could optimize operation in a variety of automated processes.
- Robotics and Drones: This transistor could be relevant in the control circuits of small robotic devices or drones, where precise switching is necessary for the operation of servos and other electronic components. Its low voltage ratings might align with the power requirements of these applications.
It is critical to note that these potential industry applications are purely conceptual and illustrative. Engineering and design teams must analyze and verify adherence to industry standards and specific application requirements before implementing these suggestions.
About Microchip Technology Inc.
Microchip Technology Inc. is a leading manufacturer in the semiconductor industry, particularly known for its extensive line of microcontrollers, analog semiconductors, memory products, and various types of transistors, including small signal bipolar transistors. The company has a robust portfolio that features not only the JANTX2N2369AUB but also a range of similar parts designed to address specific needs in electronics design.
Microchip’s products, including small signal transistors, are engineered to meet a wide variety of application requirements, ensuring high performance, reliability, and compliance with industry standards. Their commitment to quality and innovation has positioned them favorably within the electronic components market.
Research Price and Stock for JANTX2N2369AUB by Microchip Technology Inc. on Findchips.com
For those interested in acquiring the JANTX2N2369AUB, it is advisable to research stock and pricing through Findchips. This resource can provide comprehensive information on the availability of the part and allow for price comparisons from various distributors.
The part has historically been available at distributors such as Master Electronics, Avnet Americas, Onlinecomponents.com, Microchip Technology Inc., Mouser Electronics, EBV Elektronik, Avnet Silica, and DigiKey. However, potential buyers should check on Findchips for the most accurate, up-to-date stock levels and pricing before proceeding with an order.